elQ model conversion - NOT image classification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

elQ model conversion - NOT image classification

Jump to solution
2,502 Views
colinbroderick
Contributor III

Can the elQ toolkit be used to convert models which are NOT used for image classification? We have a model that produces a continuous output and there is therefore no sensible concepts of labels, but the conversion will not succeed without providing a labels file, at least in the graphical tool.

Can anyone offer advice or resources for workflows that do NOT involve image classification? It is frustratingly hard to make progress because virtually all training resources and documents and example code assume the image classification case.

In particular, at the moment, we're most interested in converting from PyTorch to ONNX. We can do this with other tools but I was keen to try out the quantization capabilities of the elQ toolkit.

Thanks

0 Kudos
Reply
1 Solution
2,492 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello colinbroderick,

 

The eIQ support Pytorch and ONNX, but it can not be used for model conversion it they are not going to use in Image classification, for this task you have the Linux BSP, where you can install an apps to do this task.

Regards

View solution in original post

0 Kudos
Reply
2 Replies
2,493 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello colinbroderick,

 

The eIQ support Pytorch and ONNX, but it can not be used for model conversion it they are not going to use in Image classification, for this task you have the Linux BSP, where you can install an apps to do this task.

Regards

0 Kudos
Reply
2,485 Views
colinbroderick
Contributor III

Ok, thanks for the answer.

0 Kudos
Reply