imx-gpu-sdk compilation stuck forever - iMX8M MiniEVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-gpu-sdk compilation stuck forever - iMX8M MiniEVK

1,195 Views
sreedhar_appala
Contributor IV

Hi,

I am trying yocto build image for iMX 8M Mini EVK.

I have followed the steps as mentioned in the https://www.nxp.com/docs/en/user-guide/i.MX_Yocto_Project_User's_Guide_Linux.pdf

>> MACHINE=imx8mmevk  DISTRO=fsl-imx-xwayland  source fsl-setup-release.sh -b build-xwayland-imx8mmevk

>>bitbake fsl-image-qt5-validation-imx

The image is starts to build and progress upto 99% and it got stuck compiling the imx-gpu-sdk.

It stuck forever. I waited for more than hour but no response.

Kindly let me know your suggestions for resolving this.

Thank you,

Sreedhar

0 Kudos
3 Replies

710 Views
NagendraB
Contributor II

hello nxp,

need to profile imx8m-mini GPU 
able to generate the .vpd file 

trying to open it in vivante VAnalyzer (v 1.5) but throwing error “unsupported data file version”
what could be the issue? any specific version to be used for imx8 mini?

0 Kudos

959 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sreedhar,

Please, remove everything and  try to download again the yocto BSP, could be a fetch problem but it is working right now.

Regards

0 Kudos

959 Views
sreedhar_appala
Contributor IV

Hi,

I tried the same and tried to build imx-linux-sumo 4.14.78-1.0.0_ga version.

I am facing the same problem.

please find the log below:

ubuntu:~/sreedhar/imx-yocto-bsp/Build-xwayland-imx8mmevk$ bitbake fsl-image-validation-imx
Loading cache: 100% |########################################################################################################################################################################| Time: 0:00:00
Loaded 3462 entries from dependency cache.
Parsing recipes: 100% |######################################################################################################################################################################| Time: 0:00:01
Parsing of 2547 .bb files complete (2546 cached, 1 parsed). 3463 targets, 219 skipped, 7 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
NOTE: Multiple providers are available for runtime ptpd (ptpd, ptpd-qoriq)
Consider defining a PREFERRED_RPROVIDER entry to match ptpd
NOTE: Multiple providers are available for runtime ptpd-dev (ptpd, ptpd-qoriq)
Consider defining a PREFERRED_RPROVIDER entry to match ptpd-dev

Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mmevk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-poky = "HEAD:64a257fa22126c4a40ff7e03424a404e360ebe1e"
meta-oe
meta-multimedia = "HEAD:2bb21ef27c4b0c9d52d30b3b2c5a0160fd02b966"
meta-freescale = "HEAD:407c6cf408969445031a492e2d25e0e2749582ea"
meta-freescale-3rdparty = "HEAD:88a29631809d1af0df618245430db29f2a7012b5"
meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"
meta-bsp
meta-sdk = "HEAD:52ac01eee49b9f2f3ffec4c4037b7928d968115b"
meta-browser = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:2bb21ef27c4b0c9d52d30b3b2c5a0160fd02b966"
meta-qt5 = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"

Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:05
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
Currently 1 running tasks (7661 of 7679) 99% |########################################################################################################################################################## |
0: imx-gpu-sdk-5.2.0-r0 do_compile - 1377s (pid 3392)

<< It stuck here for more than 90mins, after that i cancelled the task CTRL+C >>

Please let us know how to resolve this asap.

thank you, sreedhar

0 Kudos