elQ model conversion - NOT image classification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

elQ model conversion - NOT image classification

ソリューションへジャンプ
2,528件の閲覧回数
colinbroderick
Contributor III

Can the elQ toolkit be used to convert models which are NOT used for image classification? We have a model that produces a continuous output and there is therefore no sensible concepts of labels, but the conversion will not succeed without providing a labels file, at least in the graphical tool.

Can anyone offer advice or resources for workflows that do NOT involve image classification? It is frustratingly hard to make progress because virtually all training resources and documents and example code assume the image classification case.

In particular, at the moment, we're most interested in converting from PyTorch to ONNX. We can do this with other tools but I was keen to try out the quantization capabilities of the elQ toolkit.

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
2,518件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello colinbroderick,

 

The eIQ support Pytorch and ONNX, but it can not be used for model conversion it they are not going to use in Image classification, for this task you have the Linux BSP, where you can install an apps to do this task.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,519件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello colinbroderick,

 

The eIQ support Pytorch and ONNX, but it can not be used for model conversion it they are not going to use in Image classification, for this task you have the Linux BSP, where you can install an apps to do this task.

Regards

0 件の賞賛
返信
2,511件の閲覧回数
colinbroderick
Contributor III

Ok, thanks for the answer.

0 件の賞賛
返信