U-Boot and kernel completes @ 3.7sec.
systemd started galcore module.
and in parallel weston started.
Weston takes 1.2sec to complete initialization.
But if we delay weston startup around 1sec in systemd then weston comepleted init in ~250ms.
find below strace.....
1344 18:22:34.215424 ioctl(13, _IOC(0, 0x75, 0x30, 0), 0xffffffca22e0) = 0
So why dev/galcore taking more time to be available?
Can we move this galcore module insertion to kernel? what is the NXP recommandation?
Why nanosleep configured to 1sec sleep? can we reduce it?
Thanks,
Arunkumar R
已解决! 转到解答。
.
Sure, you can build the galcore.ko into kernel as build-in. In the latest Linux BSP, it's set as build-in by default.
Best regards,
Danwei
Hello,
May I ask which part number you are working with? -Because it was tagged many variants of the i.MX8 in the thread. Also, please confirm if it is an evaluation board or a custom one?
One more question, may I ask if you already have an FAE assigned or if you are already in touch with an internal NXP expert?
Thank you.
BR,
Ivan.
Hi Ivan,
We are working with imx8qx.
It is a custom board.
and rao.mr@nxp.com
Use to support us.
Thanks,
Arunkumar R
.
Sure, you can build the galcore.ko into kernel as build-in. In the latest Linux BSP, it's set as build-in by default.
Best regards,
Danwei