efuse values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

efuse values

1,363 Views
jameshe1
Contributor II

Dear all,

   Is there a right efuse config file from NXP which is verified on SABREAUTO board. i design my board almost same as SABREAUTO board except that i use ECSPI1_SS2 as CS of SPI flash. I want to a reference efuse configuation to modify for my board. I'm afraid the chip can't run well if i program wrong value, and the efuse is otp. thanks.

Labels (2)
0 Kudos
Reply
1 Reply

1,265 Views
igorpadykov
NXP Employee
NXP Employee

Hi James

I am afraid such fuse file is not available, in general one can

read SABREAUTO board boot settings in SRC_SBMR1,2 register

then use these settings for burning fuses.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply