efuse values

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

efuse values

1,422 次查看
jameshe1
Contributor II

Dear all,

   Is there a right efuse config file from NXP which is verified on SABREAUTO board. i design my board almost same as SABREAUTO board except that i use ECSPI1_SS2 as CS of SPI flash. I want to a reference efuse configuation to modify for my board. I'm afraid the chip can't run well if i program wrong value, and the efuse is otp. thanks.

标签 (2)
0 项奖励
回复
1 回复

1,324 次查看
igorpadykov
NXP Employee
NXP Employee

Hi James

I am afraid such fuse file is not available, in general one can

read SABREAUTO board boot settings in SRC_SBMR1,2 register

then use these settings for burning fuses.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复