eMMC support for iMX6 Linux BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC support for iMX6 Linux BSP

ソリューションへジャンプ
3,870件の閲覧回数
honeysukesan
Contributor II

Hi all,

I am a newbie in iMX platform.

I would like to know about the availability of eMMC NAND flash support in iMX6 BSP.

As per the i.MX_6Dual6Quad_Linux_Reference_Manual.pdf, the MMC Linux driver supports eMMC4.4 SDR and DDR modes.

Does it mean eMMC is supported in accessing NAND flash also?

As per Micron technical document e·MMC Linux Enablement, I understood that a platform specific host layer is needed

in the Linux kernel. Is this layer supported for iMX6 platform controllers in iMX6 BSP?

Thanks,

Honey S

ラベル(3)
タグ(4)
1 解決策
2,650件の閲覧回数
Paul_Kang
NXP Employee
NXP Employee

Hi Honey,

I think you are conused with eMMC and NAND. Usually, eMMC means NAND flash with controller including ECC and it is  connected thru SDHC. But NAND, usually it is refered as 'raw NAND', is pure NAND device which can be connected GPMI I/F of i.MX6. And our internal BCH block can be used for its operation.

eMMC can be connected thru uSDHC I/F and it is supported by our BSP.

Best regards,

Paul

元の投稿で解決策を見る

2 返答(返信)
2,651件の閲覧回数
Paul_Kang
NXP Employee
NXP Employee

Hi Honey,

I think you are conused with eMMC and NAND. Usually, eMMC means NAND flash with controller including ECC and it is  connected thru SDHC. But NAND, usually it is refered as 'raw NAND', is pure NAND device which can be connected GPMI I/F of i.MX6. And our internal BCH block can be used for its operation.

eMMC can be connected thru uSDHC I/F and it is supported by our BSP.

Best regards,

Paul

2,651件の閲覧回数
honeysukesan
Contributor II

Dear all,

Could anyone please put a reply to this post?

I am waiting for your reply. It's so urgent. please..

Thanks,

Honey S

0 件の賞賛
返信