eFuse lock bits with random setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eFuse lock bits with random setting

1,733 Views
jschoen
Contributor III

We are seeing an occasional issue where efuse address 0, OTP Bank0 Word0 (Lock controls), i.e., shadow register OCOTP_LOCK, does not contain the factory default value of 0x20220002.  Maybe 2 or 3 out of 100 processors will have other random bits set causing, for example the Ethernet MAC address to be locked and not writable.  We have seen 0x20220003, 0x20220012, 0x 20220202.

We are reading and writing the fuses through a version of u-boot that is loaded over USB during factory test.  Thinking that u-boot’s efuse write function may have a bug, we added code to read the lock fuse before doing any fuse writes and we are reading bit errors there too making us think the processors may be coming from Freescale with random lock bits set in error.

Has anyone else seen anything like this problem before?

0 Kudos
Reply
2 Replies

1,425 Views
jschoen
Contributor III

This is for i.MX6Q

0 Kudos
Reply

1,425 Views
lily_zhang
NXP Employee
NXP Employee

hello,

Can you please provide more details?

1. Which U-boot version you are using?

2. What's your part numbers you are using?

3. What's your detailed steps to do fuse blown/read testing? Do you have full memory fuse dump information?

0 Kudos
Reply