MCIMX6SL camera problem afte idling.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6SL camera problem afte idling.

Jump to solution
2,070 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a problem on MCIMX6SLEVK.

Actually, MCIMX6SLEVK camera input does not works correctly after about 10 min from boot.

Please see the detail as below.

=====

[Board]

MCIMX6SLEVK

[BSP]

L3.0.35_4.1.0

[Condition]

1. A camera is connected to J24 connector on MCIMX6SLEVK.

2. Camera capture and I2C3 communication to the camera work continuously.

[Procedure]

1. Boot MCIMX6SLEVK with L3.0.35_4.1.0 BSP.

2. Leave MCIMX6SLEVK idle about 10 minutes.

[Problem]

After idling, sometime I2C3 SCL is pulled "low" and I2C communication does not work well.

Additionally, capturing from a camera which is connected to J24 and uses I2C3 does not work well.

(lack some frame, and jumble capture image)

=====

[Q]

Do you have a information about similar issue?

If you have it, could you tell me what should we modify?

If you need more information, please tell me it.

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (2)
0 Kudos
Reply
1 Solution
1,921 Views
satoshishimoda
Senior Contributor I

Hi all,

I found the root cause.

It was caused by bus frequency scaling.

After about 10 min, set_low_bus_freq() and reduce_bus_freq_handler() function in /linux-3.0.35/arch/arm/mach-mx6/bus_freq.c is called.

Maybe, the reduced bus frequency is not sufficient to work camera and I2C.

We can avoid this issue by commenting out "reduce_bus_freq_handler()" or disable CONFIG_CPU_FREQ_GOV_POWERSAVE when building.

Best Regards,

Satoshi Shimoda

View solution in original post

0 Kudos
Reply
1 Reply
1,922 Views
satoshishimoda
Senior Contributor I

Hi all,

I found the root cause.

It was caused by bus frequency scaling.

After about 10 min, set_low_bus_freq() and reduce_bus_freq_handler() function in /linux-3.0.35/arch/arm/mach-mx6/bus_freq.c is called.

Maybe, the reduced bus frequency is not sufficient to work camera and I2C.

We can avoid this issue by commenting out "reduce_bus_freq_handler()" or disable CONFIG_CPU_FREQ_GOV_POWERSAVE when building.

Best Regards,

Satoshi Shimoda

0 Kudos
Reply