dts setting for wl1831

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

dts setting for wl1831

1,060 次查看
vivektol
Contributor I

Is it compulsary to apply patches for WL1831 in imx6-kernel version 3.14.52 and if yes where we will get patches ?

标签 (4)
0 项奖励
回复
1 回复

938 次查看
vinodmaverickr0
Contributor IV

I think 3.14 kernel does not have support for the WL1831 device tree binding.  However you can search the same on your device tree with the string "WL12*".

It should be something like the below string in your device tree.

compatible = "ti,wl1271"; instead of wl1831

It depends upon on you if you are using using the device tree then you need to apply the patches.

You can take the patches from the below links

[PATCH v6 5/6] ARM: dts: add wl12xx/wl18xx bindings 

[v5,2/3] wl18xx: add basic device-tree support - Patchwork 

Thanks,

Vinod

0 项奖励
回复