dts setting for wl1831

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dts setting for wl1831

1,054 Views
vivektol
Contributor I

Is it compulsary to apply patches for WL1831 in imx6-kernel version 3.14.52 and if yes where we will get patches ?

Labels (4)
0 Kudos
Reply
1 Reply

932 Views
vinodmaverickr0
Contributor IV

I think 3.14 kernel does not have support for the WL1831 device tree binding.  However you can search the same on your device tree with the string "WL12*".

It should be something like the below string in your device tree.

compatible = "ti,wl1271"; instead of wl1831

It depends upon on you if you are using using the device tree then you need to apply the patches.

You can take the patches from the below links

[PATCH v6 5/6] ARM: dts: add wl12xx/wl18xx bindings 

[v5,2/3] wl18xx: add basic device-tree support - Patchwork 

Thanks,

Vinod

0 Kudos
Reply