dsi display abnormality

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dsi display abnormality

3,229件の閲覧回数
billshih
Contributor I

hello,

I am using mipi dsi lcd.

but sometimes it randomly has the phenomenon as shown in the file attached.

I am using imx6qdl cpu.

Does anyone know ways to solve this situation?

Or any comment

Thank you.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

3,073件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Bill

such behaviour may be caused by internal buses limit,

one can try to decrease LCD fps,bpp or use processor

with higher speed grade. Also one can try to disable low power

mode with kernel boot parameter enable_wait_mode=off.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,073件の閲覧回数
billshih
Contributor I

Hello, igorpady kov

Thank you for your comment

But I don't understand...

Why disabling low power mode can be helpful? Because the device need low power mode to send power-on commends to the lcd.

Do you recommand to use high speed mode to send the power-on commends?

Because I once heard that using low power to send commends is more stable...

What do you think?

Best regards

Bill

0 件の賞賛
返信

3,073件の閲覧回数
mohammedazlum
Contributor IV

Hello,

Please share the LCD datasheet and which interface you used for integrating this LCD ?

Regards,

Azlum

0 件の賞賛
返信