dsi display abnormality

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dsi display abnormality

3,252 Views
billshih
Contributor I

hello,

I am using mipi dsi lcd.

but sometimes it randomly has the phenomenon as shown in the file attached.

I am using imx6qdl cpu.

Does anyone know ways to solve this situation?

Or any comment

Thank you.

Labels (3)
0 Kudos
Reply
3 Replies

3,096 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bill

such behaviour may be caused by internal buses limit,

one can try to decrease LCD fps,bpp or use processor

with higher speed grade. Also one can try to disable low power

mode with kernel boot parameter enable_wait_mode=off.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,096 Views
billshih
Contributor I

Hello, igorpady kov

Thank you for your comment

But I don't understand...

Why disabling low power mode can be helpful? Because the device need low power mode to send power-on commends to the lcd.

Do you recommand to use high speed mode to send the power-on commends?

Because I once heard that using low power to send commends is more stable...

What do you think?

Best regards

Bill

0 Kudos
Reply

3,096 Views
mohammedazlum
Contributor IV

Hello,

Please share the LCD datasheet and which interface you used for integrating this LCD ?

Regards,

Azlum

0 Kudos
Reply