does i.mx6DQ support eMMC 5.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

does i.mx6DQ support eMMC 5.0?

ソリューションへジャンプ
2,184件の閲覧回数
zhiminwan
Contributor I

is it OK to directly connect I.mx6 to eMMC 5.0?  the datahseet only mentions eMMC 4.4.

and if it works, does it support to directly boot from the eMMC 5.0?

thanks

ラベル(3)
0 件の賞賛
返信
1 解決策
1,821件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhimin

yes, one can connect I.mx6 with eMMC 5.0

processor will work (and boot) with it as with eMMC 4.4

Re: i.mx6 with eMMC 5.0 SDR or DDR interface?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,822件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi zhimin

yes, one can connect I.mx6 with eMMC 5.0

processor will work (and boot) with it as with eMMC 4.4

Re: i.mx6 with eMMC 5.0 SDR or DDR interface?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,821件の閲覧回数
jiwongpark
Contributor I
0 件の賞賛
返信