does i.mx6DQ support eMMC 5.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does i.mx6DQ support eMMC 5.0?

Jump to solution
2,202 Views
zhiminwan
Contributor I

is it OK to directly connect I.mx6 to eMMC 5.0?  the datahseet only mentions eMMC 4.4.

and if it works, does it support to directly boot from the eMMC 5.0?

thanks

Labels (3)
0 Kudos
Reply
1 Solution
1,839 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhimin

yes, one can connect I.mx6 with eMMC 5.0

processor will work (and boot) with it as with eMMC 4.4

Re: i.mx6 with eMMC 5.0 SDR or DDR interface?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,840 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhimin

yes, one can connect I.mx6 with eMMC 5.0

processor will work (and boot) with it as with eMMC 4.4

Re: i.mx6 with eMMC 5.0 SDR or DDR interface?

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,839 Views
jiwongpark
Contributor I
0 Kudos
Reply