display wrong after run tslib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

display wrong after run tslib

1,696 Views
bool_
Contributor I

Hello,Community:

I am now working on Freescale  imx6q   connected a 7" 800 x 480 LCD display and touch with tsc2007, i change the file .dtis .

if i use a  mouse the display is ok ,the touch can work but not the correct position.  but if i run the ts_calibrate int /usr/bin  first i can calibrate the touch panel,but after ts_calibrate quit the lcd has a wrong display, the command cat .bmp bf0 also display wrong ,but if i run ts_calibrate or ts_test,the lcd is ok.

Labels (1)
0 Kudos
Reply
2 Replies

1,583 Views
b36401
NXP Employee
NXP Employee

Are you using LCD in "rotated" mode?
Please try to play with xrandr prior to ts_calibrate.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,583 Views
bool_
Contributor I

thankyou for your answer, my lcd was not in "rotated" mode.you can see my pictures of the screen. when i run ts_calibrate the screen will be ok again

befor_calibrate.jpgdo_calibrate.jpgafter_calibrate.jpg

0 Kudos
Reply