disabling gui application on start up on imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

disabling gui application on start up on imx6

1,055件の閲覧回数
anhn
Contributor I

Is there any way to disable the gui application on start up on the imx6? if so, what are the steps?

I'm running the freescale yocto project image (Linux-4.1.15-6QP+gf295a56).

ラベル(3)
0 件の賞賛
返信
1 返信

978件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Anh

do you mean splashscreen, then one can check defines 

CONFIG_SPLASH_SCREEN in uboot/include/configs folder

uboot-imx.git - Freescale i.MX u-boot Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信