disabling gui application on start up on imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

disabling gui application on start up on imx6

1,041 Views
anhn
Contributor I

Is there any way to disable the gui application on start up on the imx6? if so, what are the steps?

I'm running the freescale yocto project image (Linux-4.1.15-6QP+gf295a56).

Labels (3)
0 Kudos
Reply
1 Reply

964 Views
igorpadykov
NXP Employee
NXP Employee

Hi Anh

do you mean splashscreen, then one can check defines 

CONFIG_SPLASH_SCREEN in uboot/include/configs folder

uboot-imx.git - Freescale i.MX u-boot Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply