disable tamper function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

disable tamper function

1,560件の閲覧回数
charleshuang
Senior Contributor II

Hi

We use internel RTC, and found that pull high tamper will increase power consumption of rtc battery

1.If we pull low this pin (disable tamper), will cause any problem?

2.How to disable/enable tamper function in software? Default function is on or off?

ラベル(4)
0 件の賞賛
返信
1 返信

1,406件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

The TAMPER pin is pulled down internally, but please check if  External Tampering is
disabled in SNVS_LPTDCR register. Correct power up sequence should be provided :
"VDD_SNVS_IN supply must be turned ON before any other power supply.
...
If a coin cell is used to power VDD_SNVS_IN, then ensure that it is connected before any other

supply is switched on."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信