disable tamper function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

disable tamper function

1,592 Views
charleshuang
Senior Contributor II

Hi

We use internel RTC, and found that pull high tamper will increase power consumption of rtc battery

1.If we pull low this pin (disable tamper), will cause any problem?

2.How to disable/enable tamper function in software? Default function is on or off?

Labels (4)
0 Kudos
Reply
1 Reply

1,438 Views
Yuri
NXP Employee
NXP Employee

Hello,

The TAMPER pin is pulled down internally, but please check if  External Tampering is
disabled in SNVS_LPTDCR register. Correct power up sequence should be provided :
"VDD_SNVS_IN supply must be turned ON before any other power supply.
...
If a coin cell is used to power VDD_SNVS_IN, then ensure that it is connected before any other

supply is switched on."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply