difference between lib

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

difference between lib

ソリューションへジャンプ
3,768件の閲覧回数
garyyin
Contributor III

In the rootfs/usr/lib generated by yocto 3.14.28. I found several versions of libGLES:

libGLES_CL.so

libGLES_CM.so

libGLESv1_CL.so

libGLESv1_CM.so

libGLESv2.so

What's the difference between these 3 versions?

What's the difference between xx_CL.so & xx_CM.so?

ラベル(5)
0 件の賞賛
返信
1 解決策
3,554件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gary

for libs description please refer to attached Linux Manual

Table 13-2. GPU Library Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,555件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Gary

for libs description please refer to attached Linux Manual

Table 13-2. GPU Library Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信