difference between lib

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

difference between lib

Jump to solution
3,772 Views
garyyin
Contributor III

In the rootfs/usr/lib generated by yocto 3.14.28. I found several versions of libGLES:

libGLES_CL.so

libGLES_CM.so

libGLESv1_CL.so

libGLESv1_CM.so

libGLESv2.so

What's the difference between these 3 versions?

What's the difference between xx_CL.so & xx_CM.so?

0 Kudos
Reply
1 Solution
3,558 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gary

for libs description please refer to attached Linux Manual

Table 13-2. GPU Library Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,559 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gary

for libs description please refer to attached Linux Manual

Table 13-2. GPU Library Files.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply