deleted

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

deleted

1,581件の閲覧回数
jayakumar2
Contributor V

deleted

ラベル(2)
0 件の賞賛
返信
1 返信

1,428件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jaya

except changing drive strength from i.MX side, it also can be changed

from EDB8132B4PM ddr: using MR3 (DS). May be useful to check temperature

dependency: if cooling down the part causes more failures, then it is likely the drive strength is
too high causing more overshoots and undershoots. Memtester differs from ddr test that

it also stresses power subsystem. One can pay attention to ripples: requirement for ripple noise

should be less than 5% Vp-p of supply voltage average value. Related power rails affected: all

VDD_xxx_IN and VDD_xxx_CAP and test with slightly increasing VDD_SOC_CAP.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信