de-interlance for yocto linux 5.10.9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

de-interlance for yocto linux 5.10.9

Jump to solution
3,109 Views
simonlin
Contributor II

Hi @qiang_li-mpu_se 

Here is my environment

HW platform: imx8-qm, tw9992

OS: Yocto Linux 5.10.9

I try to post de-interlance mode in yocto linux 5.10.9, but the V4L2 data structure is different with  below reference article

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ISL79987-and-adv7180-de-interlace-driver...

Do you have newer de-interlance patch for yocto linux 5.10.9 ?

Thanks

0 Kudos
Reply
1 Solution
3 Replies
3,097 Views
qiang_li-mpu_se
NXP Employee
NXP Employee
0 Kudos
Reply
3,101 Views
simonlin
Contributor II

Hi @qiang_li-mpu_se 

That's good news

I look forward to get the patch

Thanks for your response

 

0 Kudos
Reply
3,105 Views
qiang_li-mpu_se
NXP Employee
NXP Employee

The patch for L5.4.70 BSP will be released in next week. 

0 Kudos
Reply