ddr calibration test on i.MX6solo using .bin file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ddr calibration test on i.MX6solo using .bin file

1,016 次查看
rameshasp
Contributor IV

Hello sir,

Currently i am working on i.MX6solo part number called MCIMX6S6AVM10AD and ddr part number called IS46TR16256AL-125KBLA2 custom board but i am not able to do ddr calibration on the board.

Could you please help me this.

Thanks & Regards,

Ramesha S P

0 项奖励
回复
1 回复

911 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ramesha

one can check ddr tool usage and possible errors on below documents

https://community.nxp.com/docs/DOC-331528 

Freescale i.MX6 DRAM Port Application Guide-DDR3 

faq on link

i.MX6 DDR Stress Test Tool V1.0.3 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复