Hi folks,
I have to update an old u-boot version to 2013.4 (because of device tree support for linux 3.16.7) at embest MarSboard, i.MX6 DL. Flashing tool is MfGTool.
old U-boot: 174 KB
new U-boot: 271 KB
Currently I have faced following issue during writing u-boot to SPI-NOR flash:
Sent command:
<CMD type="push" body="$ dd if=$FILE of=/dev/mtd0 bs=512">write Emb u-boot loader to SPI-NOR</CMD>
Answer:
dd: writing '/dev/mtd0': No space left on device
257+0 records in
256+0 records out
262144 bytes (256.0KB) copied, 8.489485 seconds, 30.2KB/s
I wonder whether I have to change the parameter bs ...or to re-configure u-boot?
I would be grateful for any hints
Ricarda
Hi,
Have you tried to flash the memory from a working Linux image? if it is possible to burn the memory then there might be an issue with the linux image mfgtool is using.
Which mftool are you using?
IMX_6DQ_MFG_TOOL
: Tool and documentation for downloading OS images to the i.MX 6Quad and i.MX6Dual.
IMX_6_MFG_L3.10.17_1.0.0_TOOL
: i.MX 6Family Manufacturing Toolkit for L3.10.17.
Best Regards,
Alejandro
Hi,
I could flash working Linux image v3.0.15 with Mfg Tool v1.6.2.050 ( windows) according to description MarS Board User Manual_V1.2.pdf. The u-boot sources are provided by embest.
Thanks for the hint to care about the MfG tool version. The linux version I have never tried ...
Additionally with respect to "262144 bytes (256.0KB) copied," I wonder whether I should re-configure the mtd partitions of SPI-NOR flash. I found the structure imx6_marsboard_spi_nor_partitions[]
in ../arch/arm/mach-mx6/board-mx6q_marsboard.c in Linux sources v3.0.15.
static struct mtd_partition imx6_marsboard_spi_nor_partitions[] = {
{
.name = "bootloader",
.offset = 0,
.size = 0x00040000,
},
But until now I have never found comparable struct in linux sources v3.16.7. Maybe different because of dtb support....
Best regards,
Ricarda