data from uart is coming in parts, and not as complete buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

data from uart is coming in parts, and not as complete buffer

2,298件の閲覧回数
neerajsharma
Contributor III

Hi, i am using ti wl1273 chip on uart with freescale imx6 based board. When waiting to recieve version info from chip, the data is recieved in parts and hence the ti driver logic fails.

Any suggestions what could be the problem..?

Log:

[ 53.791790] (stk) : st_kim_start

[ 53.909975] (stk) :ldisc_install = 1

[ 53.915072] (stc): st_tty_open

[ 53.918518] (stk) :line discipline installed

[ 53.922760] <out<01 01 10 00

[ 53.926859] >in>04

[ 53.929021] >in>0e 0c 01 01 10 00 06 00 00 06 0d 00 0f 1f

Here dat being recieved comes in parts 04 and then the remaining part. This is causing problems.

I am using uart5 with ctsrts and sdma.

6 返答(返信)

2,067件の閲覧回数
neerajsharma
Contributor III

@@ -788,6 +788,7 @@ static void dma_rx_work(struct work_struct *w)

        struct imx_port *sport = container_of(w, struct imx_port, tsk_dma_rx);

        struct tty_struct *tty = sport->port.state->port.tty;

+       printk("%s uart: %d rx bytes %d\n",__FUNCTION__, sport->port.line, sport

        if (sport->rx_bytes) {

                tty_insert_flip_string(tty, sport->rx_buf, sport->rx_bytes);

@@ -1063,8 +1065,9 @@ static int imx_startup(struct uart_port *port)

        temp |= UCR1_RRDYEN | UCR1_RTSDEN | UCR1_UARTEN;

        if (sport->enable_dma) {

                temp |= UCR1_RDMAEN | UCR1_TDMAEN;

-               /* ICD,await 4 idle frames also enable AGING Timer */

-               temp |= UCR1_ICD_REG(0)|UCR1_ATDMAEN;

+               /* ICD,await 32 idle frames. Disabling AGING Timer */

+               temp |= UCR1_ICD_REG(3) ;

+               temp &= ~(UCR1_ATDMAEN);

        }

The above change in kernel/drivers/tty/serial/imx.c seems to resolve the problem, but if printk is removed the problem starts appearing again.

Can someone from freescale help me in identifying the real cause ?

2,067件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

It could be related to the stack. Would it be possible to have some charts of the signals to see how they are behaving?

0 件の賞賛
返信

2,067件の閲覧回数
neerajsharma
Contributor III

hi ,

which stack are you refereing to ?

I am using TI-st driver in kernel, along with ti uim-sys service, bluedroid, and libbt-vendor-ti.c

0 件の賞賛
返信

2,067件の閲覧回数
saurabh206
Senior Contributor III

Hi,

Neeraj

First verify signal response using scope on CTS,RTS,RX and TX pins.

If above settings are proper than you should able to get data correctly.

Thanks

Saurabh

0 件の賞賛
返信

2,067件の閲覧回数
neerajsharma
Contributor III

verified CTS, RTS, RX, TX.

0 件の賞賛
返信

2,066件の閲覧回数
neerajsharma
Contributor III

@@ -788,6 +788,7 @@ static void dma_rx_work(struct work_struct *w)

        struct imx_port *sport = container_of(w, struct imx_port, tsk_dma_rx);

        struct tty_struct *tty = sport->port.state->port.tty;

+       printk("%s uart: %d rx bytes %d\n",__FUNCTION__, sport->port.line, sport

        if (sport->rx_bytes) {

                tty_insert_flip_string(tty, sport->rx_buf, sport->rx_bytes);

@@ -1063,8 +1065,9 @@ static int imx_startup(struct uart_port *port)

        temp |= UCR1_RRDYEN | UCR1_RTSDEN | UCR1_UARTEN;

        if (sport->enable_dma) {

                temp |= UCR1_RDMAEN | UCR1_TDMAEN;

-               /* ICD,await 4 idle frames also enable AGING Timer */

-               temp |= UCR1_ICD_REG(0)|UCR1_ATDMAEN;

+               /* ICD,await 32 idle frames. Disabling AGING Timer */

+               temp |= UCR1_ICD_REG(3) ;

+               temp &= ~(UCR1_ATDMAEN);

        }

The above change in kernel/drivers/tty/serial/imx.c seems to resolve the problem, but if printk is removed the problem starts appearing again.

Can someone from freescale help me in identifying the real cause ?