core-image-minimal with OpenCL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

core-image-minimal with OpenCL

2,867 Views
erikraynolds
Contributor IV

per build core-image-minimal I do not have available OpenCL for my imx8 device. What to configure Yocto build for to enable OpenCL?

0 Kudos
Reply
2 Replies

2,626 Views
erikraynolds
Contributor IV

How to build it to include gpu driver as well  So after build there is opencl library. I guess it requires modification of local.conf. Can you describe how? 

0 Kudos
Reply

2,622 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erik

as described in Table 1. i.MX Yocto project images attached Yocto Guide

core-image-minimal is small image that only allows a device to boot.

One can try to build xwayland with gpu drivers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply