core-image-minimal with OpenCL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

core-image-minimal with OpenCL

2,877 次查看
erikraynolds
Contributor IV

per build core-image-minimal I do not have available OpenCL for my imx8 device. What to configure Yocto build for to enable OpenCL?

标记 (3)
0 项奖励
回复
2 回复数

2,636 次查看
erikraynolds
Contributor IV

How to build it to include gpu driver as well  So after build there is opencl library. I guess it requires modification of local.conf. Can you describe how? 

0 项奖励
回复

2,632 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Erik

as described in Table 1. i.MX Yocto project images attached Yocto Guide

core-image-minimal is small image that only allows a device to boot.

One can try to build xwayland with gpu drivers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复