core-image-minimal with OpenCL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

core-image-minimal with OpenCL

2,868件の閲覧回数
erikraynolds
Contributor IV

per build core-image-minimal I do not have available OpenCL for my imx8 device. What to configure Yocto build for to enable OpenCL?

0 件の賞賛
返信
2 返答(返信)

2,627件の閲覧回数
erikraynolds
Contributor IV

How to build it to include gpu driver as well  So after build there is opencl library. I guess it requires modification of local.conf. Can you describe how? 

0 件の賞賛
返信

2,623件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Erik

as described in Table 1. i.MX Yocto project images attached Yocto Guide

core-image-minimal is small image that only allows a device to boot.

One can try to build xwayland with gpu drivers.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信