codec configuration for IMX6SoloX board.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

codec configuration for IMX6SoloX board.

2,557 次查看
robinsingh
Contributor III

HI All,

I want to know the setting required for a new codec to make it work in imx6sx kernel 3.10.

here is what i am trying to do :

1) Connection :

LCD1_RESET -> AUD3_RXD   ->  -> I2S_SDIO  codec side

LCD1_ENABLE -> AUD3_TXC   -> J -> I2S_ LRCLK codec side

LCD1_HSYNC -> AUD3_TXD   ->  -> I2S_ SDI codec

LCD1_VSYNC -> AUD3_TXFS   ->  -> I2S_SCLK_codec

i have written a Machine driver(based on wm8962 driver   imx-wm8962.c) for my codec , but as of now i do not see any signal coming out:

Here is my DT binding:

============================================

/*DT binding for DAI LINK driver*/

        sound {

                compatible = "fsl,imx6q-sabresd-wm8962",

                           "fsl,imx-audio-mycodec";

                model = "mycodec-audio";

                cpu-dai = <&ssi2>; /* si-controller*/

                audio-codec = <&codec;

                audio-routing =

                        "Headphone Jack", "HPOUTL",

                        "Headphone Jack", "HPOUTR",

                        "Ext Spk", "SPKOUTL",

                        "Ext Spk", "SPKOUTR",

                        "AMIC", "MICBIAS",

                        "IN3R", "AMIC";

                mux-int-port = <2>;

                mux-ext-port = <3>;

                hp-det-gpios = <&gpio1 17 1>;

        };

==============================================

FIle : imx6sx.dtsi

audmux {

                 pinctrl_audmux_4: audmuxgrp-4 {

                        fsl,pins = <

                                MX6SX_PAD_LCD1_ENABLE__AUDMUX_AUD3_TXC  0x130B0

                                MX6SX_PAD_LCD1_VSYNC__AUDMUX_AUD3_TXFS  0x130B0

                                MX6SX_PAD_LCD1_HSYNC__AUDMUX_AUD3_TXD    0x120B0

                                MX6SX_PAD_LCD1_RESET__AUDMUX_AUD3_RXD    0x130B0

                        >;

                };

=====================

File : imx6sx-sdb.dts

&audmux {

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_audmux_4>;

        status = "okay";

};

===========================

I am using SSI2 ===>  AUD3 ====> my codec

Does above setting looks fine or i am missing something? please  share some details including clock for ssi2 etc

thanks

Robin Singh

标签 (3)
标记 (3)
0 项奖励
回复
4 回复数

2,046 次查看
igorpadykov
NXP Employee
NXP Employee

Hi robin

suggest to check attached Porting Guide

Chapter 8 Porting Audio Codecs to a Custom Board

Best regards

igor

0 项奖励
回复

2,046 次查看
saurabh206
Senior Contributor III

Hi

Robin

Does You codec is in slave configuration or master configuration?

You need to make code change for clock supply.

Thanks

Saurabh

0 项奖励
回复

2,046 次查看
robinsingh
Contributor III

HI Saurabh,

Thank you for your reply. I am configuring codec as a slave device.  what are code change required for clock supply ? Can you please give me some pointer ?

I checked in /sys/kernel/debugs/clk/clk_summry and clocks are not enable on my board for audio [ ssi1_ipg,ssi2_ipg,ssi_ipg].i tried to enable them machine code , but no luck.  please give me some pointer .

thanks

Robin Singh

0 项奖励
回复

2,046 次查看
saurabh206
Senior Contributor III

Hi

Robin

you can study existing code from "kernel\sound\soc\fsl"

Following modification is required for your driver.

snd_soc_dai_set_fmt needs to pass SND_SOC_DAIFMT_CBS_CFS for I2S as a master mode.

And

snd_soc_dai_set_sysclk(cpu_dai, 0, bclk, SND_SOC_CLOCK_OUT);

I hope this helps.

Thanks

Saurabh

0 项奖励
回复