DDR3 measurements for iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 measurements for iMX6

1,600 Views
emil
Contributor III

I'm working on a design with iMX6 that uses DDR3 memory. I'm wondering if it's recommended to do oscilloscope measurements on the DDR3 bus to verify its robustness, or if it is sufficient to just see that it is possible to read and write from it.

Thanks for your help!

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,270 Views
SergioSolis
NXP Employee
NXP Employee

Hello Emil,

Well, like the old saying, "the more the merrier"


It would be a good idea to look at the eye diagram to check the strength of the signal.

You could also do the DDR3 stress test for the i.MX6 (attached).

0 Kudos
Reply

1,270 Views
raymondyen
Contributor I

I'm testing a embedded SBC using imx6Q5, with 1G of DDR3.  RAM Stress Test failed DSQ cal.  What oscilloscope is recommended fro checking eye-diagram?

0 Kudos
Reply