changes in uboot(yocto) source are not reflecting on board(apalis-imx6q)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

changes in uboot(yocto) source are not reflecting on board(apalis-imx6q)

跳至解决方案
1,489 次查看
sumish_ks
Contributor II

Hi community,

i am trying to test a change in uboot that in uboot source file(apalis_imx6q.c) when i removed "sd-card" configuration and after that i have compiled(without error) it, i noticed that my board is getting boot properly so i just wanted to ask why this changes are not reflecting back on the board and  i am just trying to learn that if i wanted to do some changes in uboot then how it will be that is why i did this. please let me know if i have do some more additional changes or does it take any default configuration.

Thanks & best regards

Sumish

1 解答
1,409 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sumish

one can check Chapter1 Porting U-Boot attached Porting Guide.

Also may be useful to ask support from vendor apalis board, toradex

Toradex - Customer Support 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,410 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Sumish

one can check Chapter1 Porting U-Boot attached Porting Guide.

Also may be useful to ask support from vendor apalis board, toradex

Toradex - Customer Support 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复