change Imx287 power prep settings in yocto project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

change Imx287 power prep settings in yocto project

跳至解决方案
1,320 次查看
ireshj
Contributor II

hi,

 

I m developing a yocto-based (kirkstone) os for a custom board with im287 chip. currently, I have a working image for imx28evk board, now i need to port it to the custom board.

there I m facing an issue with changing the power prep settings as the custom board should not check on the battery voltage, but the uboot for the imx28evk falls to start as there's no battery in the custom board.

I went through imx porting guide and imx yocto projects user guide but could not figure out where to apply the power prep settings

much appreciated if anyone can point where to look

标签 (2)
0 项奖励
回复
1 解答
1,315 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello ireshj,

Sorry, NXP does not have continues with yocto on MX28 since kernel 3.10, and now you are in kirkstone you have to go with community BSP:

https://www.yoctoproject.org/community/

 

Regards

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,316 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello ireshj,

Sorry, NXP does not have continues with yocto on MX28 since kernel 3.10, and now you are in kirkstone you have to go with community BSP:

https://www.yoctoproject.org/community/

 

Regards

 

0 项奖励
回复