SABRE for Automotive Infotainment Based on the i.MX 6 Series : uuu flashing issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE for Automotive Infotainment Based on the i.MX 6 Series : uuu flashing issue

943 Views
vimal8327
Contributor I

Hello All,

Need some infomation regarding SABRE for Automotive
Infotainment Based on the i.MX 6 Series: uuu flashing. 

I have the following board IMX6SABREINFOQSG.pdf .I need to boot from MMC (no sd card). I have made the switch as mentioned in the document. Devices goes to recovery mode also and uuu script is used to flash. Serial console is opened, so while running the uboot log should come right, it is not coming. UUU script is also stuck (1/2). 

does /IMX6SABREINFOQSG  has on board mmc...? How to proceed forward

Note:

Used yocto to make , machine name= imx6qsabresd

0 Kudos
Reply
4 Replies

934 Views
vimal8327
Contributor I

UUU commands

sudo uuu -v u-boot-imx6qsabresd.imx

sudo uuu -d u-boot-imx6qsabresd.imx

With these command i am expecting u-boot log in the UART debug port.

 

Linux BSP version you have built using Yocto?

linux-imx : 5.15.32

DISTRO command used

DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source imx-setup-release.sh -b build

 

Please see the below switch mode, i have selected MMC flash/boot

Boot mode switch value:

S2 

S2:1= OFFS2:2 = ONS2:3 = ONS2:4 = OFF

 

S1

S1:1 = OFFS1:2 = ONS1:3 = OFFS1:4 = OFFS1:5 = ONS1:6 = ONS1:7 = OFFS1:8 = OFFS1:9 =OFFS1:10 =OFF

 

S3

S3:1 = OFFS3:2 = ONS3:3 = OFFS3:4 = ON
0 Kudos
Reply

924 Views
AldoG
NXP TechSupport
NXP TechSupport

Hi,

Thank you for providing such detailed information.

From this, I see that you have built using the i.MX6Q Sabre as MACHINE, this will create all files for the SABRESD board, this image will not boot on sabre automotive.

Unfortunately i.MX6 sabre automotive has been dropped from Yocto due to end of life, so it is not possible to select the imx6qsabreauto machine to build it.

It may be possible to build using standalone method as specified in the i.MX Poting Guide
https://www.nxp.com/docs/en/user-guide/IMX_PORTING_GUIDE.pdf

Also, for a quick start you may try with last released pre-built image (L5.10.72_2.2.2)
https://www.nxp.com/webapp/Download?colCode=L5.10.72_2.2.2_MX6QDLSOLOX&appType=license

Best regards,
Aldo.

0 Kudos
Reply

910 Views
vimal8327
Contributor I

Thank you for information.  let me try from my side

0 Kudos
Reply

940 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the UUU command you have used?
Also, please share the Linux BSP version you have built using Yocto?

Best regards,
Aldo.

0 Kudos
Reply