Hi,
I can not save parameters into SD in boot in IMX6QSD with bellow SD, but i use the classc 4 SD is ok, any limits with bellow SD or my mistake ?
TOSHIBA EXCERIA Type Ⅱ SDHC-16G UHS/CL10 R95M W60M
I want to use speeder SD to start up my image :smileysad:
U-Boot > printenv
baudrate=115200
boot_fdt=try
bootcmd=mmc dev ${mmcdev};if mmc rescan; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi
bootdelay=1
bootscript=echo Running bootscript from mmc ...; source
console=ttymxc0
ethact=FEC
ethaddr=00:04:9f:02:6f:9e
ethprime=FEC
fdt_addr=0x11000000
fdt_file=imx6q-sabresd.dtb
fdt_high=0xffffffff
initrd_high=0xffffffff
ip_dyn=yes
loadaddr=0x12000000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}
loaduimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${uimage}
mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;
mmcdev=1
mmcpart=1
mmcroot=/dev/mmcblk1p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${uimage}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootm ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootm; else echo WARN: Cannot load the DT; fi; fi; else bootm; fi;
script=boot.scr
stderr=serial
stdin=serial
stdout=serial
uimage=uImage
Environment size: 1691/8188 bytes
U-Boot > setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=${mmcroot} video=mxcfb1:off video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 dmfc=3'
U-Boot > saveenv
Saving Environment to MMC...
MMC partition switch failed
U-Boot > saveenv
Saving Environment to MMC...
Writing to MMC(1)... failed
U-Boot >
Solved! Go to Solution.
This issue is fixed by yocto branch dora duto my testing :smileyhappy:
 
					
				
		
Hi Jojo, I have a sabresd board here and with mainline u-boot I can save the env to SD without a problem. Is this what you are trying to achieve ?
As Vladan notes, the ERROR in your post above is not related to saving env to SD.
This issue is fixed by yocto branch dora duto my testing :smileyhappy:
 
					
				
		
 VladanJovanovic
		
			VladanJovanovic
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Try inserting the SD card to the other SD slot and boot from it (you will have to change boot device in boot switches in SW6 as well).
You're probably booting from MMC 0 or 2 (don't remember right now how u-boot numers them), and u-boot is trying to save to MMC 1.
Hi,
I switch to SD2 to boot up, but it's failed as bellow, how to setup the boot line ?
U-Boot 2013.04-00053-g08868db (Sep 12 2013 - 11:15:29)
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: MX6Q-SabreSD
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
MMC: no card present
MMC init failed
Using default environment
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Warning: FEC using MAC address from net device
Hit any key to stop autoboot: 0
MMC: no card present
mmc1(part 0) is current device
MMC: no card present
Booting from net ...
FEC Waiting for PHY auto negotiation to complete. done
BOOTP broadcast 1
DHCP client bound to address 192.168.10.238
Using FEC device
TFTP from server 0.0.0.0; our IP address is 192.168.10.238; sending through gateway 192.168.10.1
Filename 'uImage'.
Load address: 0x12000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#####
3 MiB/s
done
Bytes transferred = 3887020 (3b4fac hex)
BOOTP broadcast 1
DHCP client bound to address 192.168.10.238
Using FEC device
TFTP from server 0.0.0.0; our IP address is 192.168.10.238; sending through gateway 192.168.10.1
Filename 'imx6q-sabresd.dtb'.
Load address: 0x11000000
Loading: *
TFTP error: 'File not found' (1)
Not retrying...
Wrong Image Format for bootm command
ERROR: can't get kernel image!
 
					
				
		
 VladanJovanovic
		
			VladanJovanovic
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Can you save parameters to SD card?
For new issue please open a new topic and close this one if solved.
In general, you can see in what step u-boot is failing, so please check if that file is available in your TFTP server's location. Unless you're using mainline kernel with device tree support, you'll probably just want to load uImage directly. follow instructions in Linux User Guide (check documentation package for Linux) to see how to load system via TFTP/NFS.
Hi,
I switch to SD2 to boot up, but it's failed as bellow, it's the same problems with SD3
U-Boot > mmc parts
Partition Map for MMC device 0 -- Partition Type: DOS
Part Start Sector Num Sectors UUID Type
1 8192 16384 000eb2b7-01 0c
2 24576 1753088 000eb2b7-02 83
U-Boot > setenv mmcdev 0
U-Boot > saveenv
Saving Environment to MMC...
MMC: no card present
MMC init failed
 
					
				
		
Are you able to write anything with mmc write to that device ?