can imx6dl support 10-bit raw RGB csc process?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can imx6dl support 10-bit raw RGB csc process?

1,328件の閲覧回数
kevinhuhui
Contributor I

I want to use ov8858 with imx6dl. ov8858 can only support output 10-bit raw RGB image.

my question is : can imx6dl support convert 10-bit raw RGB to other color space,for exp, raw rgb --> yuv, or raw rgb --> rgb888 ?

thks.

ラベル(4)
0 件の賞賛
返信
3 返答(返信)

1,147件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kevin

in general it can, using conversion matrix described in sect.37.4.5.4

Main Processing Section i.MX6DQ Reference Manual (rev.3  7/2015)

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,147件の閲覧回数
kevinhuhui
Contributor I

HI igor

     thank you for your reply.

     the 10bit raw rgb format for ov8858  is BG/GR bayer.

     can you give me the matrix example for BG/GR to yuv conversion?

0 件の賞賛
返信

1,147件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi kevin

one can look at csc examples below and modify for own needs, if necessary

https://community.freescale.com/docs/DOC-94961

~igor

0 件の賞賛
返信