boot strapping timing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

boot strapping timing

ソリューションへジャンプ
3,677件の閲覧回数
inmaku
Contributor III

What is the Timing relation ship between sampling the i.MX6 GPIOs for boot strapping and the POR_B Signal? What are teh Setup/hold requirements?

Thanks,

Ingo

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,324件の閲覧回数
Yuri
NXP Employee
NXP Employee

I am afraid - no, this information is not provided in documentation.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,324件の閲覧回数
Yuri
NXP Employee
NXP Employee


The boot mode pins are read at 300us to 1ms after reset is deasserted,

therefore if buffers are used to isolate the boot pins, they should be

enabled for 1-10 ms after reset negation.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,324件の閲覧回数
inmaku
Contributor III

Hi Yuri,

Thanks - that is what I needed. Can I find this Information in the reference Manual or data sheet?

Thanks,

Ingo

0 件の賞賛
返信
3,325件の閲覧回数
Yuri
NXP Employee
NXP Employee

I am afraid - no, this information is not provided in documentation.

0 件の賞賛
返信
3,324件の閲覧回数
inmaku
Contributor III

After your posting I did remember one reference design making this statement: The MCIMX6SLEVK board has this note on page 13.

With this  - I guess - I have to take the word on it.

Thanks!