boot Linux and Android Auto operating systems on imx8qm mek

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

boot Linux and Android Auto operating systems on imx8qm mek

2,338件の閲覧回数
zhaocq
Contributor II

i want to boot Linux and Android Auto operating systems on imx8qm mek. As the file "i.MX Virtualization User's Guide", if i use xen mode, boot Linux and Android Auto operating systems. The last step, after the board boots into Linux OS, i need to use command "xl create /etc/xen/domu-imx8qm-mek-androidauto.cfg" to start Android OS. Coud you tell me if the tool "xl creat" need to be installed? or it don't need to install because xen linux OS DOM0 has the xen tools?

ラベル(1)
0 件の賞賛
返信
1 返信

2,128件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I’m afraid that i.MX8QM is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 件の賞賛
返信