boot Linux and Android Auto operating systems on imx8qm mek

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot Linux and Android Auto operating systems on imx8qm mek

2,800 Views
zhaocq
Contributor II

i want to boot Linux and Android Auto operating systems on imx8qm mek. As the file "i.MX Virtualization User's Guide", if i use xen mode, boot Linux and Android Auto operating systems. The last step, after the board boots into Linux OS, i need to use command "xl create /etc/xen/domu-imx8qm-mek-androidauto.cfg" to start Android OS. Coud you tell me if the tool "xl creat" need to be installed? or it don't need to install because xen linux OS DOM0 has the xen tools?

0 Kudos
Reply
1 Reply

2,590 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

I’m afraid that i.MX8QM is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos
Reply