bitbake yocto question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake yocto question

1,397 Views
hnxylhb
Contributor I

WARNING: Failed to fetch URL http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true, attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 8, output:

http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin:

2015-07-13 09:22:58 ERROR 404: Not Found.

ERROR: Function failed: Fetcher failure for URL: 'http://www.freescale.com/lgfiles/NMG/MAD/YOCTO//imx-test-hdcp-3.10.17-1.0.0.bin;fsl-eula=true'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: /home/jishuxing/fsl-arm-yocto-bsp/build/tmp/work/riotboard-poky-linux-gnueabi/imx-test-hdcp/3.10.17-1.0.0-r0/temp/log.do_fetch.3692

ERROR: Task 1667 (/home/jishuxing/fsl-arm-yocto-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-bsp/imx-test/imx-test-hdcp_3.10.17-1.0.0.bb, do_fetch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 2351 tasks of which 2350 didn't need to be rerun and 1 failed.

No currently running tasks (2350 of 4013)

Labels (2)
0 Kudos
Reply
1 Reply

944 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello roc li,

Would you please provide more information on this error? Which BSP are you using and which images or packages are you baking? I’m curious because the binaries are not being downloaded from the gits but from Freescale.com

0 Kudos
Reply