bitbake image for mys6ul14x14 error: Could not include required file recipes-fsl

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bitbake image for mys6ul14x14 error: Could not include required file recipes-fsl

ソリューションへジャンプ
2,448件の閲覧回数
totalit
Contributor III

I got the following error attempting to "bitbake core-image-base" for mys6ul14x14:

ERROR: ParseError at /home/totalit/MYS6ULx-devel/fsl-release-yocto/sources/meta-myir-imx6ulx/recipes-fsl/images/fsl-image-gui.bb:4: Could not include required file recipes-fsl/images/fsl-image-validation-imx.bb

I tried to copy this file from meta-fsl-bsp-release directory, but it entails another error.

I'm using MYS-6ULX full package and didn't modify any file except bblayers (it can't find the machine folder without it).

ラベル(2)
0 件の賞賛
返信
1 解決策
2,436件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello totallit,

Please Don't do that; this is ugly! You can get similar result using: IMAGE_FEATURES += "tools-sdk" in your local.conf and building: bitbake fsl-image-multimedia .On the other hand, the fsl-image*.bb image recipes are under sources/meta-fsl-demos/recipes-fsl/images/

Try to download the version 5.10.35 of the BSP and follow up the Yocto User guide document to run yocto on MX6ULL.

 

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,437件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello totallit,

Please Don't do that; this is ugly! You can get similar result using: IMAGE_FEATURES += "tools-sdk" in your local.conf and building: bitbake fsl-image-multimedia .On the other hand, the fsl-image*.bb image recipes are under sources/meta-fsl-demos/recipes-fsl/images/

Try to download the version 5.10.35 of the BSP and follow up the Yocto User guide document to run yocto on MX6ULL.

 

Regards

 

0 件の賞賛
返信
2,408件の閲覧回数
totalit
Contributor III

Finally, I've created an image using the last BSP and according to Yocto User guide (instead of MYS packages and MYS linux guide). Thank you for the tip!

0 件の賞賛
返信