bitbake fsl-image-gui issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitbake fsl-image-gui issue

2,143 次查看
veeranjaneyulug
Contributor III

User1@FSETBLR1LX045:~/epdc/yocto/fsl-release-bsp/build-imx6q$ bitbake fsl-image-gui

Loading cache: 100% |##########################################################################################################| ETA:  00:00:00

Loaded 2193 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

NOTE: preferred version 3.0.35-4.1.0 of xf86-video-imxfb-vivante not available (for item xserver-xorg-extension-viv-hdmi)

NOTE: versions of xf86-video-imxfb-vivante available: 3:3.10.53-1.1.0

NOTE: preferred version 3.0.35-4.1.0 of imx-kobs not available (for item imx-kobs)

NOTE: versions of imx-kobs available: 3.10.17-1.0.0 3.10.53-1.1.0

NOTE: preferred version 3.10.53-1.1.0 of imx-lib not available (for item imx-lib)

NOTE: versions of imx-lib available: 1:3.0.35-4.0.0 1:3.10.17-1.0.0

NOTE: preferred version 3.0.35-4.1.0 of xf86-video-imxfb-vivante not available (for item xf86-video-imxfb-vivante-dev)

NOTE: versions of xf86-video-imxfb-vivante available: 3:3.10.17-1.0.1 3:3.10.53-1.1.0

NOTE: preferred version 3.0.35-4.1.0 of xf86-video-imxfb-vivante not available (for item xf86-video-imxfb-vivante)

NOTE: versions of xf86-video-imxfb-vivante available: 3:3.10.17-1.0.1 3:3.10.53-1.1.0

NOTE: preferred version 3.0.35-4.1.0 of imx-kobs not available (for item imx-kobs-dev)

NOTE: versions of imx-kobs available: 3.10.17-1.0.0 3.10.53-1.1.0

NOTE: preferred version 3.10.53-1.1.0 of imx-lib not available (for item imx-lib)

NOTE: versions of imx-lib available: 1:3.0.35-4.0.0 1:3.10.17-1.0.0

NOTE: preferred version 3.10.53-1.1.0 of imx-lib not available (for item imx-lib-dev)

NOTE: versions of imx-lib available: 1:3.0.35-4.0.0 1:3.10.17-1.0.0

NOTE: multiple providers are available for jpeg-native (jpeg-native, libjpeg-turbo-native)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg-native

Build Configuration:

BB_VERSION        = "1.22.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.6.2"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):30b8d9378b8260e452552b806610dc9b6fe0b69f"

meta-oe           = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"

meta-fsl-arm      = "(nobranch):9bc540eec9a7e280af13371ea70650fcc47ea627"

meta-fsl-arm-extra = "(nobranch):e1085deb3d915d2a95a65cceadc77c6de0dadfb6"

meta-fsl-demos    = "(nobranch):f141c7d1158b8addbd6f1ed047a1b47c2ed85f8f"

meta-fsl-arm     

meta-fsl-demos    = "(nobranch):0c5367e963b5f7797ded59f835313466b896d7e9"

meta-browser      = "(nobranch):63963cc56c8d0291779693e62b66cb16e5c86883"

meta-gnome       

meta-networking  

meta-ruby         = "(nobranch):8065dd8456913457a0114ddb2b4bd4842847b2a3"

meta-qt5          = "(nobranch):c29c317e0f22202bfaa85329a580564bbc179089"

meta-fsl-qt5     

meta-fsl-bluez    = "(nobranch):0c5367e963b5f7797ded59f835313466b896d7e9"

NOTE: Preparing runqueue

ERROR: Multiple .bb files are due to be built which each provide virtual/libgles1 (/home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/imx-gpu-viv/imx-gpu-viv_5.0.11.p4.1-hfp.bb /home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-arm/recipes-graphics/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q_3.10.17-1.0.1-hfp.bb).

This usually means one provides something the other doesn't and should.

ERROR: Multiple .bb files are due to be built which each provide virtual/libgles2 (/home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/imx-gpu-viv/imx-gpu-viv_5.0.11.p4.1-hfp.bb /home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-arm/recipes-graphics/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q_3.10.17-1.0.1-hfp.bb).

This usually means one provides something the other doesn't and should.

ERROR: Multiple .bb files are due to be built which each provide virtual/libgal-x11 (/home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/imx-gpu-viv/imx-gpu-viv_5.0.11.p4.1-hfp.bb /home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-arm/recipes-graphics/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q_3.10.17-1.0.1-hfp.bb).

This usually means one provides something the other doesn't and should.

ERROR: Multiple .bb files are due to be built which each provide virtual/libgl (/home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/imx-gpu-viv/imx-gpu-viv_5.0.11.p4.1-hfp.bb /home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-arm/recipes-graphics/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q_3.10.17-1.0.1-hfp.bb).

This usually means one provides something the other doesn't and should.

ERROR: Multiple .bb files are due to be built which each provide virtual/wayland-egl (/home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/imx-gpu-viv/imx-gpu-viv_5.0.11.p4.1-hfp.bb /home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-arm/recipes-graphics/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q_3.10.17-1.0.1-hfp.bb).

This usually means one provides something the other doesn't and should.

ERROR: Multiple versions of xf86-video-imxfb-vivante are due to be built (/home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/xorg-driver/xf86-video-imxfb-vivante_3.10.53-1.1.0.bb /home/User1/epdc/yocto/fsl-release-bsp/sources/meta-fsl-arm/recipes-graphics/xorg-driver/xf86-video-imxfb-vivante_3.10.17-1.0.1.bb). Only one version of a given PN should be built in any given build. You likely need to set PREFERRED_VERSION_xf86-video-imxfb-vivante to select the correct version or don't depend on multiple versions.

Summary: There were 6 ERROR messages shown, returning a non-zero exit code.

标签 (6)
0 项奖励
回复
2 回复数

1,245 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Veeranjaneyulu,

Would you please confirm which BSP Release version are you using? I would also make sure that the local.conf file has the EULA acceptance set to 1.

Sometimes it can also help to make a clean all.

  $ bitbake –c cleanall fsl-image-gui

0 项奖励
回复

1,245 次查看
veeranjaneyulug
Contributor III

We used 3.14.28 version. The above error came from using this command bitbake gstreamer1.0-plugins-imx. 

0 项奖励
回复