bitbake debug mode (-DDD) no errors

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

bitbake debug mode (-DDD) no errors

4,035 次查看
arsadhusainmomi
Contributor I

Hi,

I have setup the yocto build system on my pc.

I'm working on i.MX 7 Dual SABRE board.

First I did

bitbake imx-test

Which fetched and built the latest imx-test package in my build directory.

What I wanted to do was,

make changes in the source code of the programs in imx-test package and compile them using bitbake.

So I made my changes and tried

bitbake -c compile -f imx-test

Which compiled the imx-test package with modified source code.

But the output binary files did not generate, because my code had some errors in it.

So I tried

bitbake -c compile -f imx-test -DDD

Which gave a lot of debug information, but none about the errors in my code.

The surprising thing was that the compile task was shown to be successful, even with the errors in my code.

But the output binaries were not generated because of the errors.

What is the highest level of debug mode in bitbake?

Is there any way to view the errors in my code using bitbake?

Please help asap.

Thanks.

标签 (3)
0 项奖励
回复
1 回复

2,616 次查看
jimmychan
NXP TechSupport
NXP TechSupport

you can read the log file in imx-test/1_5.7-r0/temp/log.do_compile

0 项奖励
回复