bitbake debug mode (-DDD) no errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake debug mode (-DDD) no errors

4,001 Views
arsadhusainmomi
Contributor I

Hi,

I have setup the yocto build system on my pc.

I'm working on i.MX 7 Dual SABRE board.

First I did

bitbake imx-test

Which fetched and built the latest imx-test package in my build directory.

What I wanted to do was,

make changes in the source code of the programs in imx-test package and compile them using bitbake.

So I made my changes and tried

bitbake -c compile -f imx-test

Which compiled the imx-test package with modified source code.

But the output binary files did not generate, because my code had some errors in it.

So I tried

bitbake -c compile -f imx-test -DDD

Which gave a lot of debug information, but none about the errors in my code.

The surprising thing was that the compile task was shown to be successful, even with the errors in my code.

But the output binaries were not generated because of the errors.

What is the highest level of debug mode in bitbake?

Is there any way to view the errors in my code using bitbake?

Please help asap.

Thanks.

Labels (3)
0 Kudos
Reply
1 Reply

2,582 Views
jimmychan
NXP TechSupport
NXP TechSupport

you can read the log file in imx-test/1_5.7-r0/temp/log.do_compile

0 Kudos
Reply