bitbake core-image-minimal failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bitbake core-image-minimal failed

3,109件の閲覧回数
jasonshao
Contributor II

Below is the log, who can tell me what can I do now.

$ bitbake core-image-minimal
Loading cache: 100% |########################################################################################################################################################################| ETA: 00:00:00
Loaded 2792 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "i686-linux"
NATIVELSBSTRING = "Ubuntu-12.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ulevk"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.1.15-2.1.0"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe
meta-multimedia = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp
meta-sdk = "HEAD:823b26a67261270d2bf22d511e6190641a8a90cf"
meta-browser = "HEAD:77736988073a5d90fcff9d0005c8477332ede387"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5 = "HEAD:ccae79be69c5268df3b47e4e14cea0591c39a531"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: gnu-config-native-20150728+gitAUTOINC+b576fa87c1-r0 do_unpack: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:
fatal: the '--set-upstream' option is no longer supported. Please use '--track' or '--set-upstream-to' instead.

ERROR: Logfile of failure stored in: /home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/work/i686-linux/gnu-config-native/20150728+gitAUTOINC+b576fa87c1-r0/temp/log.do_unpack.22970
Log data follows:
| DEBUG: Executing python function do_unpack
| DEBUG: Executing python function base_do_unpack
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-bH0aIL4376,guid=10957f8723fd13851939038800000022"; export SSH_AGENT_PID="1873"; export SSH_AUTH_SOCK="/tmp/keyring-RKux5C/ssh"; export PATH="/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts/native-intercept:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin/i686-linux:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/sbin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/sbin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/bin:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/bitbake/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/home/jason/bin"; export HOME="/home/jason"; git -c core.fsyncobjectfiles=0 clone -s -n /home/jason/bin/fsl-arm-yocto-bsp/downloads//git2/git.sv.gnu.org.config.git/ /home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/work/i686-linux/gnu-config-native/20150728+gitAUTOINC+b576fa87c1-r0/git/
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-bH0aIL4376,guid=10957f8723fd13851939038800000022"; export SSH_AGENT_PID="1873"; export SSH_AUTH_SOCK="/tmp/keyring-RKux5C/ssh"; export PATH="/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts/native-intercept:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin/i686-linux:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/sbin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/sbin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/bin:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/bitbake/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/home/jason/bin"; export HOME="/home/jason"; git -c core.fsyncobjectfiles=0 remote set-url origin git://git.sv.gnu.org/config.git
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-bH0aIL4376,guid=10957f8723fd13851939038800000022"; export SSH_AGENT_PID="1873"; export SSH_AUTH_SOCK="/tmp/keyring-RKux5C/ssh"; export PATH="/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts/native-intercept:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin/i686-linux:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/sbin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/sbin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/bin:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/bitbake/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/home/jason/bin"; export HOME="/home/jason"; git -c core.fsyncobjectfiles=0 checkout -B master b576fa87c140b824466ef1638e945e87dc5c0343
| DEBUG: Running export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-bH0aIL4376,guid=10957f8723fd13851939038800000022"; export SSH_AGENT_PID="1873"; export SSH_AUTH_SOCK="/tmp/keyring-RKux5C/ssh"; export PATH="/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts/native-intercept:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin/i686-linux:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/sbin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/usr/bin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/sbin:/home/jason/bin/fsl-arm-yocto-bsp/build-fb/tmp/sysroots/i686-linux/bin:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/scripts:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/bitbake/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/home/jason/bin"; export HOME="/home/jason"; git -c core.fsyncobjectfiles=0 branch --set-upstream master origin/master
| DEBUG: Python function base_do_unpack finished
| DEBUG: Python function do_unpack finished
| ERROR: Function failed: Fetcher failure: Fetch command failed with exit code 128, output:
| fatal: the '--set-upstream' option is no longer supported. Please use '--track' or '--set-upstream-to' instead.
|
ERROR: Task 310 (virtual:native:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_git.bb, do_unpack) failed with exit code '1'
NOTE: Tasks Summary: Attempted 35 tasks of which 31 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
virtual:native:/home/jason/bin/fsl-arm-yocto-bsp/sources/poky/meta/recipes-devtools/gnu-config/gnu-config_git.bb, do_unpack
Summary: There was 1 ERROR message shown, returning a non-zero exit code.

ラベル(3)
2 返答(返信)

2,321件の閲覧回数
jasonshao
Contributor II

I have solved the problem myself.

0 件の賞賛
返信

2,321件の閲覧回数
ypyao
Contributor I

Hi Mr. Shao

    how to solve this problem? I have encounted it. look forward to you, Thanks!

0 件の賞賛
返信