i.MX6 Dual Plus Power Consumption Measurement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 Dual Plus Power Consumption Measurement

1,441 Views
neilwinlee
NXP Employee
NXP Employee

Hi,

I found AN4576_Rev.1.pdf which is i.MX6 dual lite version.

Do you have it for i.MX6DualPlus?

Best Regards,

Neil

Labels (1)
0 Kudos
Reply
1 Reply

1,313 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Neil,

There is not a dedicated Application Note for the i.MX6 Dual Plus power consumption. However, there is an application note (AN5381) in which the current consumption of the i.MX6QP is measured. (Which may help assess the i.MX6DP current consumption). You may find it on the following link:

https://www.nxp.com/docs/en/application-note/AN5381.pdf

It is not as detailed as AN4509 but it should serve as a guidelines for what power consumption to expect when using the i.MX6 Plus variants.

Regards,

0 Kudos
Reply