audio testing on imx8mmevk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

audio testing on imx8mmevk board

1,590 Views
ganesh_k
Contributor III

Hi Team,

        I m trying to test the audio on imx8mmevk. currently flashed prebuilt multimedia images(L5.4.47-2.2.0_images_MX8MMEVK). i can able to play the audio file in the terminal without error but unable to listen the sound(connected headphones at J401 connector). Please check the below logs.

root@imx8mmevk:~# aplay WAV_1Mb.wav
Playing WAVE 'WAV_1Mb.wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo

root@imx8mmevk:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: imxspdif [imx-spdif], device 0: S/PDIF PCM snd-soc-dummy-dai-0 [S/PDIF PCM snd-soc-dummy-dai-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 2: btscoaudio [bt-sco-audio], device 0: 30020000.sai-bt-sco-pcm bt-sco-pcm-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
card 3: wm8524audio [wm8524-audio], device 0: 30030000.sai-wm8524-hifi wm8524-hifi-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0

Please suggest any docs or methods to test the audio.

Thanks in advance

0 Kudos
Reply
1 Reply

1,587 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

 

for testing audio one can also try configurations described in

sect.7.5 Audio Mixer (AUDMIX)  i.MX Linux Reference Manual​

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_amix_test?h=lf-5.10.y_1.0.0

 

Best regards
igor

0 Kudos
Reply