asymmetric cryptography operations (ECDSA) with Linux imx-5.10.35-2.0.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

asymmetric cryptography operations (ECDSA) with Linux imx-5.10.35-2.0.0

1,500 Views
matteo-facchinetti
Contributor II

Hi,

In Linux, I need to use openssl + cryptodev module to use for asymmetric cryptography operations (ECDSA) with the iMX8QM CAAM module.

For the old kernel version, I have used the AN12838 as example and I would like to use a similar way also for 5.10 but I don't find the relatad kernel module patch.

What's the status of the ECDSA support in the current kernel version?
This patch, for the Linux 5.4, can be used for production, or is a simple example.... Why is not integrated in the BSP?

0 Kudos
Reply
2 Replies

1,455 Views
Yuri
NXP Employee
NXP Employee

@matteo-facchinetti 
Hello,

    We'll update the BSP security chapter guide for the next BSP.

Regards,
Yuri.

0 Kudos
Reply

1,485 Views
Yuri
NXP Employee
NXP Employee

@matteo-facchinetti 
Hello,

  I've sent You some comments directly.

Regards,
Yuri.

0 Kudos
Reply