asymmetric cryptography operations (ECDSA) with Linux imx-5.10.35-2.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

asymmetric cryptography operations (ECDSA) with Linux imx-5.10.35-2.0.0

1,499 次查看
matteo-facchinetti
Contributor II

Hi,

In Linux, I need to use openssl + cryptodev module to use for asymmetric cryptography operations (ECDSA) with the iMX8QM CAAM module.

For the old kernel version, I have used the AN12838 as example and I would like to use a similar way also for 5.10 but I don't find the relatad kernel module patch.

What's the status of the ECDSA support in the current kernel version?
This patch, for the Linux 5.4, can be used for production, or is a simple example.... Why is not integrated in the BSP?

0 项奖励
回复
2 回复数

1,454 次查看
Yuri
NXP Employee
NXP Employee

@matteo-facchinetti 
Hello,

    We'll update the BSP security chapter guide for the next BSP.

Regards,
Yuri.

0 项奖励
回复

1,484 次查看
Yuri
NXP Employee
NXP Employee

@matteo-facchinetti 
Hello,

  I've sent You some comments directly.

Regards,
Yuri.

0 项奖励
回复